Package | Description |
---|---|
nxopen.formboard |
Provides interfaces and classes to the Routing Electrical Formboard functionality.
|
Modifier and Type | Field and Description |
---|---|
static FlipComponentBuilder.AxisType |
FlipComponentBuilder.AxisType.CUSTOM
Flip component by user defined custom axis
|
static FlipComponentBuilder.AxisType |
FlipComponentBuilder.AxisType.PATH_LOCATIONS
Flip component by path locations
|
Modifier and Type | Method and Description |
---|---|
FlipComponentBuilder.AxisType |
FlipComponentBuilder.axisTypeEnum()
Returns the user selected
FlipComponentBuilder.AxisType method
License requirements: routing_harness ("Routing Harness") Created in NX7.5.0 |
static FlipComponentBuilder.AxisType |
FlipComponentBuilder.AxisType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlipComponentBuilder.AxisType |
FlipComponentBuilder.AxisType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlipComponentBuilder.AxisType[] |
FlipComponentBuilder.AxisType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FlipComponentBuilder.setAxisTypeEnum(FlipComponentBuilder.AxisType axisTypeEnum)
License requirements: routing_harness ("Routing Harness") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.