Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static StepBuilder.StepLocations |
StepBuilder.StepLocations.END
Step is located on one side of a face.
|
static StepBuilder.StepLocations |
StepBuilder.StepLocations.MIDDLE
Step is located on middle of two boudary curves
|
Modifier and Type | Method and Description |
---|---|
StepBuilder.StepLocations |
StepBuilder.stepLocation()
Returns the step location
License requirements: nx_aero_design (" NX Aero Design") . |
static StepBuilder.StepLocations |
StepBuilder.StepLocations.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StepBuilder.StepLocations |
StepBuilder.StepLocations.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StepBuilder.StepLocations[] |
StepBuilder.StepLocations.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
StepBuilder.setStepLocation(StepBuilder.StepLocations stepLocation)
License requirements: nx_aero_design (" NX Aero Design") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.