public static class StepBuilder.StepLocations extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_END
Step is located on one side of a face.
|
static int |
_MIDDLE
Step is located on middle of two boudary curves
|
static StepBuilder.StepLocations |
END
Step is located on one side of a face.
|
static StepBuilder.StepLocations |
MIDDLE
Step is located on middle of two boudary curves
|
Modifier and Type | Method and Description |
---|---|
static StepBuilder.StepLocations |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static StepBuilder.StepLocations |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static StepBuilder.StepLocations[] |
values()
Returns an array that contains the values for this enum.
|
public static final StepBuilder.StepLocations END
public static final StepBuilder.StepLocations MIDDLE
public static final int _END
public static final int _MIDDLE
public static StepBuilder.StepLocations valueOf(int value)
public static StepBuilder.StepLocations valueOf(String name)
public static StepBuilder.StepLocations[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.