Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.BROKEN_EXTRACT
The extracted feature curves have been converted with no constraints, because the selected feature has a broken extract
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.BROKEN_LINK
The linked feature curves have been converted with no constraints, because the selected feature has a broken link
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.BROKEN_LINK_NULL_XFORM
The linked feature is missing some linking data and will be treated as a broken link.
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.EXTRACT_SOME_CONSTRAINTS_NOT_TRANSFERRED
The extracted feature curves have been converted, but without some constraints
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.EXTRACT_SOURCE_SUPPRESSED
The extracted feature curves have been converted with no constraints, because a source feature of the selected feature is suppressed.
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.INVALID_FEATURE
This feature type cannot be converted into an independent sketch
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.INVALID_INPUT
The input entity is not a feature
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.LINKED_CURVE_DIFFERENT_FROM_SOURCE_CURVE
The linked feature has at least one linked curve whose geometry is different than its source curve.
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.MULTIPLE_COPLANAR_SKETCHES
This composite curve feature is based on multiple coplanar source sketches.
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.MULTIPLE_CURVES_JOINED_INTO_ONE_LINKED_CURVE
The linked feature has atleast one linked curve that is the result of joining multiple source curves.
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.MULTIPLE_INSTANCE_OF_ASOURCE_PART
The linked feature has at least two linked curves that come from multiple instances of the same source part.
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.MULTIPLE_SKETCHES_WITH_NON_PARALLEL_NORMALS
The linked feature has curves that come from multiple sketches whose plane normals are not parallel.
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.MULTIPLE_XFORM
The linked feature has multiple linking data.
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.NO_ISSUES
The linked feature curves have been converted with no issues
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.NOT_PLANAR
This feature cannot be converted into an independent sketch.
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.OUT_OF_DATE
The linked feature curves have been converted with no constraints, because the selected feature had an out-of-date link
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.OUT_OF_DATE_EXTRACT
The extracted feature curves have been converted with no constraints, because the selected feature had an out-of-date extract
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.SINGLE_SOURCE_MULTIPLE_LINKS
The linked Composite Curve feature has multiple curves linked to the same source curve.
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.SOME_CONSTRAINTS_NOT_TRANSFERRED
The linked feature curves have been converted, but without some constraints
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.SOURCE_NOT_LOADED
The linked feature curves have been converted with no constraints, because the source part for the selected feature is not loaded
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.SOURCE_SUPPRESSED
The linked feature curves have been converted with no constraints, because a source feature of the selected feature is suppressed.
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.SUPPRESSED
A suppressed feature cannot be converted into an independent sketch
|
Modifier and Type | Method and Description |
---|---|
SketchConversionStatus.ReasonType |
SketchConversionStatus.reason()
Returns the reason for failed or partially succeeded conversion of a linked-feature to
an independent sketch
License requirements: None. |
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SketchConversionStatus.ReasonType |
SketchConversionStatus.ReasonType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SketchConversionStatus.ReasonType[] |
SketchConversionStatus.ReasonType.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.