public static class SketchConversionStatus.ReasonType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_BROKEN_EXTRACT
The extracted feature curves have been converted with no constraints, because the selected feature has a broken extract
|
static int |
_BROKEN_LINK
The linked feature curves have been converted with no constraints, because the selected feature has a broken link
|
static int |
_BROKEN_LINK_NULL_XFORM
The linked feature is missing some linking data and will be treated as a broken link.
|
static int |
_EXTRACT_SOME_CONSTRAINTS_NOT_TRANSFERRED
The extracted feature curves have been converted, but without some constraints
|
static int |
_EXTRACT_SOURCE_SUPPRESSED
The extracted feature curves have been converted with no constraints, because a source feature of the selected feature is suppressed.
|
static int |
_INVALID_FEATURE
This feature type cannot be converted into an independent sketch
|
static int |
_INVALID_INPUT
The input entity is not a feature
|
static int |
_LINKED_CURVE_DIFFERENT_FROM_SOURCE_CURVE
The linked feature has at least one linked curve whose geometry is different than its source curve.
|
static int |
_MULTIPLE_COPLANAR_SKETCHES
This composite curve feature is based on multiple coplanar source sketches.
|
static int |
_MULTIPLE_CURVES_JOINED_INTO_ONE_LINKED_CURVE
The linked feature has atleast one linked curve that is the result of joining multiple source curves.
|
static int |
_MULTIPLE_INSTANCE_OF_ASOURCE_PART
The linked feature has at least two linked curves that come from multiple instances of the same source part.
|
static int |
_MULTIPLE_SKETCHES_WITH_NON_PARALLEL_NORMALS
The linked feature has curves that come from multiple sketches whose plane normals are not parallel.
|
static int |
_MULTIPLE_XFORM
The linked feature has multiple linking data.
|
static int |
_NO_ISSUES
The linked feature curves have been converted with no issues
|
static int |
_NOT_PLANAR
This feature cannot be converted into an independent sketch.
|
static int |
_OUT_OF_DATE
The linked feature curves have been converted with no constraints, because the selected feature had an out-of-date link
|
static int |
_OUT_OF_DATE_EXTRACT
The extracted feature curves have been converted with no constraints, because the selected feature had an out-of-date extract
|
static int |
_SINGLE_SOURCE_MULTIPLE_LINKS
The linked Composite Curve feature has multiple curves linked to the same source curve.
|
static int |
_SOME_CONSTRAINTS_NOT_TRANSFERRED
The linked feature curves have been converted, but without some constraints
|
static int |
_SOURCE_NOT_LOADED
The linked feature curves have been converted with no constraints, because the source part for the selected feature is not loaded
|
static int |
_SOURCE_SUPPRESSED
The linked feature curves have been converted with no constraints, because a source feature of the selected feature is suppressed.
|
static int |
_SUPPRESSED
A suppressed feature cannot be converted into an independent sketch
|
static SketchConversionStatus.ReasonType |
BROKEN_EXTRACT
The extracted feature curves have been converted with no constraints, because the selected feature has a broken extract
|
static SketchConversionStatus.ReasonType |
BROKEN_LINK
The linked feature curves have been converted with no constraints, because the selected feature has a broken link
|
static SketchConversionStatus.ReasonType |
BROKEN_LINK_NULL_XFORM
The linked feature is missing some linking data and will be treated as a broken link.
|
static SketchConversionStatus.ReasonType |
EXTRACT_SOME_CONSTRAINTS_NOT_TRANSFERRED
The extracted feature curves have been converted, but without some constraints
|
static SketchConversionStatus.ReasonType |
EXTRACT_SOURCE_SUPPRESSED
The extracted feature curves have been converted with no constraints, because a source feature of the selected feature is suppressed.
|
static SketchConversionStatus.ReasonType |
INVALID_FEATURE
This feature type cannot be converted into an independent sketch
|
static SketchConversionStatus.ReasonType |
INVALID_INPUT
The input entity is not a feature
|
static SketchConversionStatus.ReasonType |
LINKED_CURVE_DIFFERENT_FROM_SOURCE_CURVE
The linked feature has at least one linked curve whose geometry is different than its source curve.
|
static SketchConversionStatus.ReasonType |
MULTIPLE_COPLANAR_SKETCHES
This composite curve feature is based on multiple coplanar source sketches.
|
static SketchConversionStatus.ReasonType |
MULTIPLE_CURVES_JOINED_INTO_ONE_LINKED_CURVE
The linked feature has atleast one linked curve that is the result of joining multiple source curves.
|
static SketchConversionStatus.ReasonType |
MULTIPLE_INSTANCE_OF_ASOURCE_PART
The linked feature has at least two linked curves that come from multiple instances of the same source part.
|
static SketchConversionStatus.ReasonType |
MULTIPLE_SKETCHES_WITH_NON_PARALLEL_NORMALS
The linked feature has curves that come from multiple sketches whose plane normals are not parallel.
|
static SketchConversionStatus.ReasonType |
MULTIPLE_XFORM
The linked feature has multiple linking data.
|
static SketchConversionStatus.ReasonType |
NO_ISSUES
The linked feature curves have been converted with no issues
|
static SketchConversionStatus.ReasonType |
NOT_PLANAR
This feature cannot be converted into an independent sketch.
|
static SketchConversionStatus.ReasonType |
OUT_OF_DATE
The linked feature curves have been converted with no constraints, because the selected feature had an out-of-date link
|
static SketchConversionStatus.ReasonType |
OUT_OF_DATE_EXTRACT
The extracted feature curves have been converted with no constraints, because the selected feature had an out-of-date extract
|
static SketchConversionStatus.ReasonType |
SINGLE_SOURCE_MULTIPLE_LINKS
The linked Composite Curve feature has multiple curves linked to the same source curve.
|
static SketchConversionStatus.ReasonType |
SOME_CONSTRAINTS_NOT_TRANSFERRED
The linked feature curves have been converted, but without some constraints
|
static SketchConversionStatus.ReasonType |
SOURCE_NOT_LOADED
The linked feature curves have been converted with no constraints, because the source part for the selected feature is not loaded
|
static SketchConversionStatus.ReasonType |
SOURCE_SUPPRESSED
The linked feature curves have been converted with no constraints, because a source feature of the selected feature is suppressed.
|
static SketchConversionStatus.ReasonType |
SUPPRESSED
A suppressed feature cannot be converted into an independent sketch
|
Modifier and Type | Method and Description |
---|---|
static SketchConversionStatus.ReasonType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SketchConversionStatus.ReasonType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SketchConversionStatus.ReasonType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SketchConversionStatus.ReasonType NO_ISSUES
public static final SketchConversionStatus.ReasonType BROKEN_LINK
public static final SketchConversionStatus.ReasonType OUT_OF_DATE
public static final SketchConversionStatus.ReasonType SOURCE_NOT_LOADED
public static final SketchConversionStatus.ReasonType SOURCE_SUPPRESSED
public static final SketchConversionStatus.ReasonType SUPPRESSED
public static final SketchConversionStatus.ReasonType NOT_PLANAR
public static final SketchConversionStatus.ReasonType INVALID_FEATURE
public static final SketchConversionStatus.ReasonType INVALID_INPUT
public static final SketchConversionStatus.ReasonType MULTIPLE_COPLANAR_SKETCHES
public static final SketchConversionStatus.ReasonType SOME_CONSTRAINTS_NOT_TRANSFERRED
public static final SketchConversionStatus.ReasonType BROKEN_LINK_NULL_XFORM
public static final SketchConversionStatus.ReasonType MULTIPLE_XFORM
public static final SketchConversionStatus.ReasonType SINGLE_SOURCE_MULTIPLE_LINKS
public static final SketchConversionStatus.ReasonType MULTIPLE_SKETCHES_WITH_NON_PARALLEL_NORMALS
public static final SketchConversionStatus.ReasonType MULTIPLE_CURVES_JOINED_INTO_ONE_LINKED_CURVE
public static final SketchConversionStatus.ReasonType LINKED_CURVE_DIFFERENT_FROM_SOURCE_CURVE
public static final SketchConversionStatus.ReasonType MULTIPLE_INSTANCE_OF_ASOURCE_PART
public static final SketchConversionStatus.ReasonType BROKEN_EXTRACT
public static final SketchConversionStatus.ReasonType OUT_OF_DATE_EXTRACT
public static final SketchConversionStatus.ReasonType EXTRACT_SOURCE_SUPPRESSED
public static final SketchConversionStatus.ReasonType EXTRACT_SOME_CONSTRAINTS_NOT_TRANSFERRED
public static final int _NO_ISSUES
public static final int _BROKEN_LINK
public static final int _OUT_OF_DATE
public static final int _SOURCE_NOT_LOADED
public static final int _SOURCE_SUPPRESSED
public static final int _SUPPRESSED
public static final int _NOT_PLANAR
public static final int _INVALID_FEATURE
public static final int _INVALID_INPUT
public static final int _MULTIPLE_COPLANAR_SKETCHES
public static final int _SOME_CONSTRAINTS_NOT_TRANSFERRED
public static final int _BROKEN_LINK_NULL_XFORM
public static final int _MULTIPLE_XFORM
public static final int _SINGLE_SOURCE_MULTIPLE_LINKS
public static final int _MULTIPLE_SKETCHES_WITH_NON_PARALLEL_NORMALS
public static final int _MULTIPLE_CURVES_JOINED_INTO_ONE_LINKED_CURVE
public static final int _LINKED_CURVE_DIFFERENT_FROM_SOURCE_CURVE
public static final int _MULTIPLE_INSTANCE_OF_ASOURCE_PART
public static final int _BROKEN_EXTRACT
public static final int _OUT_OF_DATE_EXTRACT
public static final int _EXTRACT_SOURCE_SUPPRESSED
public static final int _EXTRACT_SOME_CONSTRAINTS_NOT_TRANSFERRED
public static SketchConversionStatus.ReasonType valueOf(int value)
public static SketchConversionStatus.ReasonType valueOf(String name)
public static SketchConversionStatus.ReasonType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.