Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.die |
Provides classes and interfaces relating to Die Engineering and Die Design.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Method and Description |
---|---|
SelectFeature |
FlatteningBuilder.selectFlatteningFeature()
Deprecated.
Deprecated in NX11.0.0. Use
FlatteningAndFormingBuilder instead.
|
Modifier and Type | Method and Description |
---|---|
SelectFeature |
SpringbackCompensationBuilder.oneStep()
Returns the one-step feature.
|
SelectFeature |
PierceTaskBuilder.tipFeature()
Returns the tip feature
License requirements: die_engineering ("DIE ENGINEERING") . |
Modifier and Type | Method and Description |
---|---|
SelectFeature |
PartGeometryCopySelectBuilder.curveFeature()
Returns the curve feature
License requirements: None. |
SelectFeature |
IsolateFeatureBuilder.feature()
Returns the Feature to Isolate
License requirements: None. |
SelectFeature |
StyledBlendBuilder.inheritFeatureParameters()
Returns a feature from which parameters will be inherited.
|
SelectFeature |
SilhouetteFlangeBuilder.parentFeature()
Returns the parent feature.
|
SelectFeature |
PaintParametersBuilder.sourceFeature()
Returns the source feature
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectFeature |
WindshieldDatumBuilder.eyeFeature()
Returns the eye feature; select eec feature when eye type specified.
|
SelectFeature |
VisionPlaneBuilder.eyeFeature()
Returns the eye feature; select eec feature when eye type specified.
|
Modifier and Type | Method and Description |
---|---|
SelectFeature |
NestModuleBuilder.destinationModule()
Deprecated.
Deprecated in NX10.0.0. Please use
FeatureCollection.reorganizeFeature(nxopen.features.Feature[], nxopen.features.Feature, nxopen.features.FeatureCollection.ReorderType) instead.
|
SelectFeature |
NestModuleBuilder.moduleToNest()
Deprecated.
Deprecated in NX10.0.0. Please use
FeatureCollection.reorganizeFeature(nxopen.features.Feature[], nxopen.features.Feature, nxopen.features.FeatureCollection.ReorderType) instead.
|
SelectFeature |
UnnestModuleBuilder.moduleToUnnest()
Deprecated.
Deprecated in NX10.0.0. Please use
FeatureCollection.reorganizeFeature(nxopen.features.Feature[], nxopen.features.Feature, nxopen.features.FeatureCollection.ReorderType) instead.
|
Modifier and Type | Method and Description |
---|---|
SelectFeature |
DieEngStampingCarryoverBuilder.dieTip()
Returns the die tip
License requirements: None. |
SelectFeature |
DieEngFormTaskBuilder.dieTip()
Returns the die tip selection.
|
SelectFeature |
DieEngTrimTaskBuilder.selectDieTip()
Returns the selected die tip.
|
Modifier and Type | Method and Description |
---|---|
SelectFeature |
JointmarkPointsBuilder.mappingFeature()
Returns the selected feature to move to the location specified.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.