Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static SectionCurveBuilder.PlaneType |
SectionCurveBuilder.PlaneType.PARALLEL
Set of planes parallel to a base plane
|
static SectionCurveBuilder.PlaneType |
SectionCurveBuilder.PlaneType.PERPENDICULAR_TO_CURVE
Set of planes perpendicular to a curve
|
static SectionCurveBuilder.PlaneType |
SectionCurveBuilder.PlaneType.RADIAL
Set of planes radiating from a base plane
|
static SectionCurveBuilder.PlaneType |
SectionCurveBuilder.PlaneType.SELECTED
Planes are selected (not specified by
one of the following methods)
|
Modifier and Type | Method and Description |
---|---|
SectionCurveBuilder.PlaneType |
SectionCurveBuilder.type()
Returns the type of the section curve builder
License requirements: None. |
static SectionCurveBuilder.PlaneType |
SectionCurveBuilder.PlaneType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionCurveBuilder.PlaneType |
SectionCurveBuilder.PlaneType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionCurveBuilder.PlaneType[] |
SectionCurveBuilder.PlaneType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionCurveBuilder.setType(SectionCurveBuilder.PlaneType type)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.