public static class SectionCurveBuilder.PlaneType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_PARALLEL
Set of planes parallel to a base plane
|
static int |
_PERPENDICULAR_TO_CURVE
Set of planes perpendicular to a curve
|
static int |
_RADIAL
Set of planes radiating from a base plane
|
static int |
_SELECTED
Planes are selected (not specified by
one of the following methods)
|
static SectionCurveBuilder.PlaneType |
PARALLEL
Set of planes parallel to a base plane
|
static SectionCurveBuilder.PlaneType |
PERPENDICULAR_TO_CURVE
Set of planes perpendicular to a curve
|
static SectionCurveBuilder.PlaneType |
RADIAL
Set of planes radiating from a base plane
|
static SectionCurveBuilder.PlaneType |
SELECTED
Planes are selected (not specified by
one of the following methods)
|
Modifier and Type | Method and Description |
---|---|
static SectionCurveBuilder.PlaneType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionCurveBuilder.PlaneType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionCurveBuilder.PlaneType[] |
values()
Returns an array that contains the values for this enum.
|
public static final SectionCurveBuilder.PlaneType SELECTED
public static final SectionCurveBuilder.PlaneType PARALLEL
public static final SectionCurveBuilder.PlaneType RADIAL
public static final SectionCurveBuilder.PlaneType PERPENDICULAR_TO_CURVE
public static final int _SELECTED
public static final int _PARALLEL
public static final int _RADIAL
public static final int _PERPENDICULAR_TO_CURVE
public static SectionCurveBuilder.PlaneType valueOf(int value)
public static SectionCurveBuilder.PlaneType valueOf(String name)
public static SectionCurveBuilder.PlaneType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.