Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static MapleBuilder.LocationType |
MapleBuilder.LocationType.OPERATING_SYSTEM
Worksheet is on the native OS file system.
|
static MapleBuilder.LocationType |
MapleBuilder.LocationType.TEAMCENTER
Worksheet is in Teamcenter.
|
Modifier and Type | Method and Description |
---|---|
MapleBuilder.LocationType |
MapleBuilder.location()
Deprecated.
Deprecated in NX12.0.0. Use
MathIntegrationBuilder instead.
|
static MapleBuilder.LocationType |
MapleBuilder.LocationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MapleBuilder.LocationType |
MapleBuilder.LocationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MapleBuilder.LocationType[] |
MapleBuilder.LocationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
MapleBuilder.setLocation(MapleBuilder.LocationType location)
Deprecated.
Deprecated in NX12.0.0. Use
MathIntegrationBuilder instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.