public static class MapleBuilder.LocationType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_OPERATING_SYSTEM
Worksheet is on the native OS file system.
|
static int |
_TEAMCENTER
Worksheet is in Teamcenter.
|
static MapleBuilder.LocationType |
OPERATING_SYSTEM
Worksheet is on the native OS file system.
|
static MapleBuilder.LocationType |
TEAMCENTER
Worksheet is in Teamcenter.
|
Modifier and Type | Method and Description |
---|---|
static MapleBuilder.LocationType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MapleBuilder.LocationType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MapleBuilder.LocationType[] |
values()
Returns an array that contains the values for this enum.
|
public static final MapleBuilder.LocationType OPERATING_SYSTEM
public static final MapleBuilder.LocationType TEAMCENTER
public static final int _OPERATING_SYSTEM
public static final int _TEAMCENTER
public static MapleBuilder.LocationType valueOf(int value)
public static MapleBuilder.LocationType valueOf(String name)
public static MapleBuilder.LocationType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.