Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static HolePackageBuilder.ThreadLengthOptions |
HolePackageBuilder.ThreadLengthOptions.CUSTOM
Length is custom
|
static HolePackageBuilder.ThreadLengthOptions |
HolePackageBuilder.ThreadLengthOptions.DIAMETERX1
1 * (tap drill diameter)
|
static HolePackageBuilder.ThreadLengthOptions |
HolePackageBuilder.ThreadLengthOptions.DIAMETERX15
1.5 * (tap drill diameter)
|
static HolePackageBuilder.ThreadLengthOptions |
HolePackageBuilder.ThreadLengthOptions.DIAMETERX20
2 * (tap drill diameter)
|
static HolePackageBuilder.ThreadLengthOptions |
HolePackageBuilder.ThreadLengthOptions.DIAMETERX25
2.5 * (tap drill diameter)
|
static HolePackageBuilder.ThreadLengthOptions |
HolePackageBuilder.ThreadLengthOptions.DIAMETERX30
3 * (tap drill diameter)
|
static HolePackageBuilder.ThreadLengthOptions |
HolePackageBuilder.ThreadLengthOptions.FULL
Length is full hole depth
|
static HolePackageBuilder.ThreadLengthOptions |
HolePackageBuilder.ThreadLengthOptions.STANDARD
Length is Standard
|
Modifier and Type | Method and Description |
---|---|
HolePackageBuilder.ThreadLengthOptions |
HolePackageBuilder.threadLengthOption()
Returns the thread length option - this is applicable for threaded hole
License requirements: None. |
static HolePackageBuilder.ThreadLengthOptions |
HolePackageBuilder.ThreadLengthOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HolePackageBuilder.ThreadLengthOptions |
HolePackageBuilder.ThreadLengthOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HolePackageBuilder.ThreadLengthOptions[] |
HolePackageBuilder.ThreadLengthOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HolePackageBuilder.setThreadLengthOption(HolePackageBuilder.ThreadLengthOptions threadLengthOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.