Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static HolePackageBuilder.HoleDepthLimitOptions |
HolePackageBuilder.HoleDepthLimitOptions.THROUGH_BODY
Through body limit options
|
static HolePackageBuilder.HoleDepthLimitOptions |
HolePackageBuilder.HoleDepthLimitOptions.UNTIL_NEXT
Until next limit options
|
static HolePackageBuilder.HoleDepthLimitOptions |
HolePackageBuilder.HoleDepthLimitOptions.UNTIL_SELECTED
Until selected limit options
|
static HolePackageBuilder.HoleDepthLimitOptions |
HolePackageBuilder.HoleDepthLimitOptions.VALUE
Value limit options
|
Modifier and Type | Method and Description |
---|---|
HolePackageBuilder.HoleDepthLimitOptions |
HolePackageBuilder.holeDepthLimitOption()
Returns the hole depth limit - this is applicable for general hole, threaded hole and drill size hole type
License requirements: None. |
static HolePackageBuilder.HoleDepthLimitOptions |
HolePackageBuilder.HoleDepthLimitOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HolePackageBuilder.HoleDepthLimitOptions |
HolePackageBuilder.HoleDepthLimitOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HolePackageBuilder.HoleDepthLimitOptions[] |
HolePackageBuilder.HoleDepthLimitOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HolePackageBuilder.setHoleDepthLimitOption(HolePackageBuilder.HoleDepthLimitOptions holeDepthLimitOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.