Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static GeometricConstraintData.ParameterDirection |
GeometricConstraintData.ParameterDirection.ISO
Iso parameter
|
static GeometricConstraintData.ParameterDirection |
GeometricConstraintData.ParameterDirection.NORMAL
Normal
|
static GeometricConstraintData.ParameterDirection |
GeometricConstraintData.ParameterDirection.PERPENDICULAR
Perpendicular to curve on face or edge
|
static GeometricConstraintData.ParameterDirection |
GeometricConstraintData.ParameterDirection.SECTION
General section if point is attached to face
|
Modifier and Type | Method and Description |
---|---|
GeometricConstraintData.ParameterDirection |
GeometricConstraintData.automaticConstraintDirection()
Returns the automatic constraint direction type.
|
static GeometricConstraintData.ParameterDirection |
GeometricConstraintData.ParameterDirection.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GeometricConstraintData.ParameterDirection |
GeometricConstraintData.ParameterDirection.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GeometricConstraintData.ParameterDirection[] |
GeometricConstraintData.ParameterDirection.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GeometricConstraintData.setAutomaticConstraintDirection(GeometricConstraintData.ParameterDirection autoConstraintDirection)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.