public static class GeometricConstraintData.ParameterDirection extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ISO
Iso parameter
|
static int |
_NORMAL
Normal
|
static int |
_PERPENDICULAR
Perpendicular to curve on face or edge
|
static int |
_SECTION
General section if point is attached to face
|
static GeometricConstraintData.ParameterDirection |
ISO
Iso parameter
|
static GeometricConstraintData.ParameterDirection |
NORMAL
Normal
|
static GeometricConstraintData.ParameterDirection |
PERPENDICULAR
Perpendicular to curve on face or edge
|
static GeometricConstraintData.ParameterDirection |
SECTION
General section if point is attached to face
|
Modifier and Type | Method and Description |
---|---|
static GeometricConstraintData.ParameterDirection |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GeometricConstraintData.ParameterDirection |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GeometricConstraintData.ParameterDirection[] |
values()
Returns an array that contains the values for this enum.
|
public static final GeometricConstraintData.ParameterDirection ISO
public static final GeometricConstraintData.ParameterDirection SECTION
public static final GeometricConstraintData.ParameterDirection NORMAL
public static final GeometricConstraintData.ParameterDirection PERPENDICULAR
public static final int _ISO
public static final int _SECTION
public static final int _NORMAL
public static final int _PERPENDICULAR
public static GeometricConstraintData.ParameterDirection valueOf(int value)
public static GeometricConstraintData.ParameterDirection valueOf(String name)
public static GeometricConstraintData.ParameterDirection[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.