Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static FlatteningAndFormingBuilderEx.Constraints |
FlatteningAndFormingBuilderEx.Constraints.FIXED_ELEMENTS |
static FlatteningAndFormingBuilderEx.Constraints |
FlatteningAndFormingBuilderEx.Constraints.NO_CONSTRAINTS |
Modifier and Type | Method and Description |
---|---|
FlatteningAndFormingBuilderEx.Constraints |
FlatteningAndFormingBuilderEx.constraintOptions()
Returns the option to minimize the disturbance
License requirements: None. |
static FlatteningAndFormingBuilderEx.Constraints |
FlatteningAndFormingBuilderEx.Constraints.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlatteningAndFormingBuilderEx.Constraints |
FlatteningAndFormingBuilderEx.Constraints.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlatteningAndFormingBuilderEx.Constraints[] |
FlatteningAndFormingBuilderEx.Constraints.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FlatteningAndFormingBuilderEx.setConstraintOptions(FlatteningAndFormingBuilderEx.Constraints constraintOptions)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.