public interface FlatteningAndFormingBuilderEx extends FeatureBuilder
FreeformSurfaceCollection.createFlatteningAndFormingBuilderEx(nxopen.features.FlatteningAndForming)
Property | Value |
---|---|
ConstraintOptions | NoConstraints |
DistortionMapOptions | None |
ReverseTransformation | 0 |
Modifier and Type | Interface and Description |
---|---|
static class |
FlatteningAndFormingBuilderEx.Constraints
No constraints options.
|
static class |
FlatteningAndFormingBuilderEx.DistortionMap
Distortion Map options.
|
static class |
FlatteningAndFormingBuilderEx.Types
Flattening Types
|
Modifier and Type | Method and Description |
---|---|
ScCollector |
auxiliaryFaces()
Returns the auxiliary faces that will be used to calculate the mapping of being flattened separatly and then connected to the flattened source faces
License requirements: None. |
FlatteningAndFormingBuilderEx.Constraints |
constraintOptions()
Returns the option to minimize the disturbance
License requirements: None. |
Section |
cutCurves()
Returns the cut curves on or close to the source face can be used to tear the source face along these curvesto reduce the distortion during flattening
License requirements: None. |
CoordinateSystem |
destinationCoordinateSystem()
Returns the coordinate system
License requirements: None. |
FlatteningAndFormingBuilderEx.DistortionMap |
distortionMapOptions()
Returns the option to display the distortion map on the source faces.
|
NXObjectList |
fixedElementsList()
Returns the list of points, curves or edges or faces of the source faces that act as fixed items
License requirements: None. |
SelectNXObject |
flatteningFeature()
Returns the flattening feature whose unwrapping mapping can be used to replay the unwrap or wrap on other objects
License requirements: None. |
SelectNXObject |
outerBoundary()
Returns the outer boundary of the source face that could have the longest length
License requirements: None. |
boolean |
reverseTransformation()
Returns the flag indicating if the reverse transformation will be used in the opposite direction
License requirements: None. |
void |
setConstraintOptions(FlatteningAndFormingBuilderEx.Constraints constraintOptions)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
void |
setDestinationCoordinateSystem(CoordinateSystem coordSystem)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
void |
setDistortionMapOptions(FlatteningAndFormingBuilderEx.DistortionMap distortionMapOptions)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
void |
setReverseTransformation(boolean reverseTransformation)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
void |
setSourceDirection(Direction sourceDirection)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
void |
setSourceOrigin(Point sourceOrigin)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
void |
setSourceVDirection(Direction sourceVDirection)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
void |
setTabDetection(boolean tabDetection)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
void |
setType(FlatteningAndFormingBuilderEx.Types type)
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Direction |
sourceDirection()
Returns the source direction determines the orientation of the flattened surface.
|
ScCollector |
sourceFaces()
Returns the source faces that will be used to calculate the mapping of being flattened
License requirements: None. |
Point |
sourceOrigin()
Returns the source origin is a point on one of the source face.
|
Direction |
sourceVDirection()
Returns the secondary direction is the cross product of primary direction and source face normal
License requirements: None. |
boolean |
tabDetection()
Returns the flag that indicates if internal tabbed faces can be shown or not.
|
SelectNXObjectList |
transformationObjects()
Returns the transformation objects are additional objects that can be flattened with the same mapping.
|
FlatteningAndFormingBuilderEx.Types |
type()
Returns the type
License requirements: None. |
commitFeature, getFeature, hideInternalParentFeatureAfterEdit, parentFeatureInternal, patchSolutionFlag, patchSurfaceFilename, setParentFeatureInternal, setParentFeatureInternal, setPatchSolutionFlag, setPatchSurfaceFilename, setSurroundingPatchSurfaceFilename, showInternalParentFeatureForEdit, surroundingPatchSurfaceFilename, unsetParentFeatureInternal
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
FlatteningAndFormingBuilderEx.Types type() throws NXException, RemoteException
NXException
RemoteException
void setType(FlatteningAndFormingBuilderEx.Types type) throws NXException, RemoteException
type
- NXException
RemoteException
ScCollector sourceFaces() throws NXException, RemoteException
NXException
RemoteException
ScCollector auxiliaryFaces() throws NXException, RemoteException
NXException
RemoteException
SelectNXObject outerBoundary() throws NXException, RemoteException
NXException
RemoteException
Point sourceOrigin() throws NXException, RemoteException
NXException
RemoteException
void setSourceOrigin(Point sourceOrigin) throws NXException, RemoteException
sourceOrigin
- NXException
RemoteException
Direction sourceDirection() throws NXException, RemoteException
NXException
RemoteException
void setSourceDirection(Direction sourceDirection) throws NXException, RemoteException
sourceDirection
- NXException
RemoteException
Section cutCurves() throws NXException, RemoteException
NXException
RemoteException
SelectNXObject flatteningFeature() throws NXException, RemoteException
NXException
RemoteException
boolean reverseTransformation() throws NXException, RemoteException
NXException
RemoteException
void setReverseTransformation(boolean reverseTransformation) throws NXException, RemoteException
reverseTransformation
- NXException
RemoteException
FlatteningAndFormingBuilderEx.Constraints constraintOptions() throws NXException, RemoteException
NXException
RemoteException
void setConstraintOptions(FlatteningAndFormingBuilderEx.Constraints constraintOptions) throws NXException, RemoteException
constraintOptions
- NXException
RemoteException
NXObjectList fixedElementsList() throws NXException, RemoteException
NXException
RemoteException
SelectNXObjectList transformationObjects() throws NXException, RemoteException
NXException
RemoteException
FlatteningAndFormingBuilderEx.DistortionMap distortionMapOptions() throws NXException, RemoteException
NXException
RemoteException
void setDistortionMapOptions(FlatteningAndFormingBuilderEx.DistortionMap distortionMapOptions) throws NXException, RemoteException
distortionMapOptions
- NXException
RemoteException
boolean tabDetection() throws NXException, RemoteException
NXException
RemoteException
void setTabDetection(boolean tabDetection) throws NXException, RemoteException
tabDetection
- NXException
RemoteException
CoordinateSystem destinationCoordinateSystem() throws NXException, RemoteException
NXException
RemoteException
void setDestinationCoordinateSystem(CoordinateSystem coordSystem) throws NXException, RemoteException
coordSystem
- NXException
RemoteException
Direction sourceVDirection() throws NXException, RemoteException
NXException
RemoteException
void setSourceVDirection(Direction sourceVDirection) throws NXException, RemoteException
sourceVDirection
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.