Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static ExtendSheetBuilder.SurfaceShape |
ExtendSheetBuilder.SurfaceShape.MIRRORED
Extends a B-surface by mirroring the curvature continuous shape of the surface.
|
static ExtendSheetBuilder.SurfaceShape |
ExtendSheetBuilder.SurfaceShape.NATURAL_CURVATURE
Extends a B-surface with a small area that is curvature continuous at the boundary, and then tangent beyond that area.
|
static ExtendSheetBuilder.SurfaceShape |
ExtendSheetBuilder.SurfaceShape.NATURAL_TANGENT
Extends a B-surface tangent from the boundary.
|
Modifier and Type | Method and Description |
---|---|
ExtendSheetBuilder.SurfaceShape |
TrimAndExtendBuilder.surfaceShapeOption()
Returns the extension method
License requirements: None. |
ExtendSheetBuilder.SurfaceShape |
ExtendSheetBuilder.surfaceShapeOption()
Returns the method by which the surface is extended which defines the shape
License requirements: None. |
static ExtendSheetBuilder.SurfaceShape |
ExtendSheetBuilder.SurfaceShape.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExtendSheetBuilder.SurfaceShape |
ExtendSheetBuilder.SurfaceShape.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExtendSheetBuilder.SurfaceShape[] |
ExtendSheetBuilder.SurfaceShape.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TrimAndExtendBuilder.setSurfaceShapeOption(ExtendSheetBuilder.SurfaceShape surfaceShapeOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
ExtendSheetBuilder.setSurfaceShapeOption(ExtendSheetBuilder.SurfaceShape surfaceShapeOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.