public static class ExtendSheetBuilder.SurfaceShape extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_MIRRORED
Extends a B-surface by mirroring the curvature continuous shape of the surface.
|
static int |
_NATURAL_CURVATURE
Extends a B-surface with a small area that is curvature continuous at the boundary, and then tangent beyond that area.
|
static int |
_NATURAL_TANGENT
Extends a B-surface tangent from the boundary.
|
static ExtendSheetBuilder.SurfaceShape |
MIRRORED
Extends a B-surface by mirroring the curvature continuous shape of the surface.
|
static ExtendSheetBuilder.SurfaceShape |
NATURAL_CURVATURE
Extends a B-surface with a small area that is curvature continuous at the boundary, and then tangent beyond that area.
|
static ExtendSheetBuilder.SurfaceShape |
NATURAL_TANGENT
Extends a B-surface tangent from the boundary.
|
Modifier and Type | Method and Description |
---|---|
static ExtendSheetBuilder.SurfaceShape |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ExtendSheetBuilder.SurfaceShape |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ExtendSheetBuilder.SurfaceShape[] |
values()
Returns an array that contains the values for this enum.
|
public static final ExtendSheetBuilder.SurfaceShape NATURAL_CURVATURE
public static final ExtendSheetBuilder.SurfaceShape NATURAL_TANGENT
public static final ExtendSheetBuilder.SurfaceShape MIRRORED
public static final int _NATURAL_CURVATURE
public static final int _NATURAL_TANGENT
public static final int _MIRRORED
public static ExtendSheetBuilder.SurfaceShape valueOf(int value)
public static ExtendSheetBuilder.SurfaceShape valueOf(String name)
public static ExtendSheetBuilder.SurfaceShape[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.