Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static EmbossLimit.EndcapMethod |
EmbossLimit.EndcapMethod.NONE
Indicates End-Cap geometry is formulated by the selected geometry without displacement.
|
static EmbossLimit.EndcapMethod |
EmbossLimit.EndcapMethod.OFFSET_APPROXIMATION
Indicates End-Cap geometry is formulated as an approximate offset of the selected End-Cap geometry
|
static EmbossLimit.EndcapMethod |
EmbossLimit.EndcapMethod.OFFSET_EXACT
Indicates End-Cap geometry is formulated as an exact offset of the selected End-Cap geometry.
|
static EmbossLimit.EndcapMethod |
EmbossLimit.EndcapMethod.TRANSLATION
Indicates End-Cap geometry is a translation along a user controlled vector.
|
Modifier and Type | Method and Description |
---|---|
EmbossLimit.EndcapMethod |
EmbossLimit.endcapOption()
Returns the endcap method to create the End-Cap
License requirements: None. |
static EmbossLimit.EndcapMethod |
EmbossLimit.EndcapMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EmbossLimit.EndcapMethod |
EmbossLimit.EndcapMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EmbossLimit.EndcapMethod[] |
EmbossLimit.EndcapMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EmbossLimit.setEndcapOption(EmbossLimit.EndcapMethod endcapOption)
Sets the endcap method to create the End-Cap
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.