public interface EmbossLimit extends TaggedObject
EmbossLimit.EndcapMethod.OFFSET_EXACT
EmbossLimit.EndcapSourceOption.TARGET
Modifier and Type | Interface and Description |
---|---|
static class |
EmbossLimit.EndcapMethod
Describes the method that can be applied to the selected geometry to define the End-Cap.
|
static class |
EmbossLimit.EndcapSourceOption
Describes the geometry that is used to create the End-Cap face/body.
|
Modifier and Type | Method and Description |
---|---|
Direction |
direction()
Returns the direction for translation
License requirements: None. |
Expression |
distance()
Returns the default distance for offset or translation
License requirements: None. |
EmbossLimit.EndcapMethod |
endcapOption()
Returns the endcap method to create the End-Cap
License requirements: None. |
EmbossLimit.EndcapSourceOption |
endcapSource()
Returns the endcap source option to decide where the End-Cap comes from
License requirements: None. |
EmbossTarget[] |
getTargets()
The emboss targets
License requirements: None. |
void |
setDirection(Direction direction)
Sets the direction for translation
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
setDistance(String distance)
The default distance expression formula string for offset or translation
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
setEndcapOption(EmbossLimit.EndcapMethod endcapOption)
Sets the endcap method to create the End-Cap
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
setEndcapSource(EmbossLimit.EndcapSourceOption endcapSourceOption)
Sets the endcap source option to decide where the End-Cap comes from
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
setTargets(EmbossTarget[] targets)
The emboss targets
License requirements: solid_modeling ("SOLIDS MODELING") . |
printTestData, printTestData, tag, tagValue
void setEndcapOption(EmbossLimit.EndcapMethod endcapOption) throws NXException, RemoteException
endcapOption
- The End-Cap method to create the End-Cap.NXException
RemoteException
EmbossLimit.EndcapMethod endcapOption() throws NXException, RemoteException
NXException
RemoteException
void setEndcapSource(EmbossLimit.EndcapSourceOption endcapSourceOption) throws NXException, RemoteException
endcapSourceOption
- The End-Cap source option to decide where the End-Cap comes from.NXException
RemoteException
EmbossLimit.EndcapSourceOption endcapSource() throws NXException, RemoteException
NXException
RemoteException
void setTargets(EmbossTarget[] targets) throws NXException, RemoteException
targets
- Array of EmbossTarget object. In NX4, only one target is supported.NXException
RemoteException
EmbossTarget[] getTargets() throws NXException, RemoteException
NXException
RemoteException
void setDirection(Direction direction) throws NXException, RemoteException
direction
- The direction for translation.NXException
RemoteException
Direction direction() throws NXException, RemoteException
NXException
RemoteException
void setDistance(String distance) throws NXException, RemoteException
distance
- The default distance expression formula string for offset or translation.NXException
RemoteException
Expression distance() throws NXException, RemoteException
NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.