Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DeleteFaceBuilder.FaceEdgeBlendPreferenceOptions |
DeleteFaceBuilder.FaceEdgeBlendPreferenceOptions.CLIFF
Delete as cliff blend.
|
static DeleteFaceBuilder.FaceEdgeBlendPreferenceOptions |
DeleteFaceBuilder.FaceEdgeBlendPreferenceOptions.NOTCH
Delete as notch blend.
|
Modifier and Type | Method and Description |
---|---|
DeleteFaceBuilder.FaceEdgeBlendPreferenceOptions |
DeleteFaceBuilder.faceEdgeBlendPreference()
Returns the preference option indicating wether to delete undetermined blend chain as notch chain or as cliff chain
License requirements: None. |
static DeleteFaceBuilder.FaceEdgeBlendPreferenceOptions |
DeleteFaceBuilder.FaceEdgeBlendPreferenceOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DeleteFaceBuilder.FaceEdgeBlendPreferenceOptions |
DeleteFaceBuilder.FaceEdgeBlendPreferenceOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DeleteFaceBuilder.FaceEdgeBlendPreferenceOptions[] |
DeleteFaceBuilder.FaceEdgeBlendPreferenceOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DeleteFaceBuilder.setFaceEdgeBlendPreference(DeleteFaceBuilder.FaceEdgeBlendPreferenceOptions faceEdgeBlendPreference)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.