public interface DeleteFaceBuilder extends FeatureBuilder
FeatureCollection.createDeleteFaceBuilder(nxopen.features.Feature)
Property | Value |
---|---|
CapOption | FaceOrPlane |
DeletePartialBlend | False |
FaceEdgeBlendPreference | Cliff |
Heal | True |
HealPlanar | False |
MaxBlendRadius.Value | 5.0 (millimeters part), 0.2 (inches part) |
MaxHoleDiameter.Value | 5.0 (millimeters part), 0.2 (inches part) |
Setback | SelectedBlend |
SpecifyBlend | False |
UseHoleDiameter | True |
Modifier and Type | Interface and Description |
---|---|
static class |
DeleteFaceBuilder.CapOptionValues
Represents the cap option values.
|
static class |
DeleteFaceBuilder.FaceEdgeBlendPreferenceOptions
Represents the face edge blend preference options.
|
static class |
DeleteFaceBuilder.SelectTypes
Enumeration of select type, don't use it until nx502 .
|
static class |
DeleteFaceBuilder.SetbackOptions
Represents the set back options.
|
Modifier and Type | Method and Description |
---|---|
ScCollector |
blendCollector()
Returns the blend collector holding the blends to delete
License requirements: None. |
SelectISurface |
capFace()
Returns the face or plane to be used as cap face.
|
DeleteFaceBuilder.CapOptionValues |
capOption()
Returns the cap option.
|
Plane |
capPlane()
Returns the new plane to be used as cap face.
|
boolean |
deletePartialBlend()
Returns the flag indicating whether to delete the partial blend or not.
|
ScCollector |
faceCollector()
Returns the face collector holding the faces to delete, don't use it until nx502
License requirements: None. |
DeleteFaceBuilder.FaceEdgeBlendPreferenceOptions |
faceEdgeBlendPreference()
Returns the preference option indicating wether to delete undetermined blend chain as notch chain or as cliff chain
License requirements: None. |
boolean |
heal()
Returns the flag specifying whether to heal the body while deleting its face.
|
boolean |
healPlanar()
Returns the flag of finding a plane in which all edges of a hole lie and attach this to a face covering the hole during heal hole process,
don't use it until further notification
License requirements: None. |
Expression |
maxBlendRadius()
Returns the maximal radius of deleted blends, only for delete blend type
License requirements: None. |
Expression |
maxHoleDiameter()
Returns the maximal diameter of deleted holes, only for delete hole type and only working when use_hole_diameter is true,
don't use it until nx502
License requirements: None. |
DeleteFaceBuilder.SetbackOptions |
setback()
Returns the set back options.
|
void |
setCapOption(DeleteFaceBuilder.CapOptionValues capOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
setCapPlane(Plane capPlane)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
setDeletePartialBlend(boolean deletePartialBlend)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
setFaceEdgeBlendPreference(DeleteFaceBuilder.FaceEdgeBlendPreferenceOptions faceEdgeBlendPreference)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") . |
void |
setHeal(boolean heal)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
setHealPlanar(boolean healPlanar)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
setSetback(DeleteFaceBuilder.SetbackOptions setback)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
setSpecifyBlend(boolean specifyBlend)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
setType(DeleteFaceBuilder.SelectTypes selectType)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
void |
setUseHoleDiameter(boolean useHoleDiameter)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
boolean |
specifyBlend()
Returns the flag of treating all input faces as blend, don't use it until further notification
License requirements: None. |
DeleteFaceBuilder.SelectTypes |
type()
Returns the delete face type, don't use it until nx502
License requirements: None. |
boolean |
useHoleDiameter()
Returns the flag of using hole diameter to filter hole or not, only for delete hole type and the max hole diameter should be
set if it is true, don't use it until nx502
License requirements: None. |
commitFeature, getFeature, hideInternalParentFeatureAfterEdit, parentFeatureInternal, patchSolutionFlag, patchSurfaceFilename, setParentFeatureInternal, setParentFeatureInternal, setPatchSolutionFlag, setPatchSurfaceFilename, setSurroundingPatchSurfaceFilename, showInternalParentFeatureForEdit, surroundingPatchSurfaceFilename, unsetParentFeatureInternal
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
DeleteFaceBuilder.SelectTypes type() throws NXException, RemoteException
NXException
RemoteException
void setType(DeleteFaceBuilder.SelectTypes selectType) throws NXException, RemoteException
selectType
- the delete face typeNXException
RemoteException
ScCollector faceCollector() throws NXException, RemoteException
NXException
RemoteException
boolean useHoleDiameter() throws NXException, RemoteException
NXException
RemoteException
void setUseHoleDiameter(boolean useHoleDiameter) throws NXException, RemoteException
useHoleDiameter
- the flag of use hole diameterNXException
RemoteException
Expression maxHoleDiameter() throws NXException, RemoteException
NXException
RemoteException
boolean specifyBlend() throws NXException, RemoteException
NXException
RemoteException
void setSpecifyBlend(boolean specifyBlend) throws NXException, RemoteException
specifyBlend
- NXException
RemoteException
boolean healPlanar() throws NXException, RemoteException
NXException
RemoteException
void setHealPlanar(boolean healPlanar) throws NXException, RemoteException
healPlanar
- NXException
RemoteException
boolean heal() throws NXException, RemoteException
NXException
RemoteException
void setHeal(boolean heal) throws NXException, RemoteException
heal
- NXException
RemoteException
DeleteFaceBuilder.CapOptionValues capOption() throws NXException, RemoteException
NXException
RemoteException
void setCapOption(DeleteFaceBuilder.CapOptionValues capOption) throws NXException, RemoteException
capOption
- NXException
RemoteException
SelectISurface capFace() throws NXException, RemoteException
NXException
RemoteException
Plane capPlane() throws NXException, RemoteException
NXException
RemoteException
void setCapPlane(Plane capPlane) throws NXException, RemoteException
capPlane
- NXException
RemoteException
boolean deletePartialBlend() throws NXException, RemoteException
NXException
RemoteException
void setDeletePartialBlend(boolean deletePartialBlend) throws NXException, RemoteException
deletePartialBlend
- NXException
RemoteException
DeleteFaceBuilder.SetbackOptions setback() throws NXException, RemoteException
NXException
RemoteException
void setSetback(DeleteFaceBuilder.SetbackOptions setback) throws NXException, RemoteException
setback
- NXException
RemoteException
Expression maxBlendRadius() throws NXException, RemoteException
NXException
RemoteException
ScCollector blendCollector() throws NXException, RemoteException
NXException
RemoteException
DeleteFaceBuilder.FaceEdgeBlendPreferenceOptions faceEdgeBlendPreference() throws NXException, RemoteException
NXException
RemoteException
void setFaceEdgeBlendPreference(DeleteFaceBuilder.FaceEdgeBlendPreferenceOptions faceEdgeBlendPreference) throws NXException, RemoteException
faceEdgeBlendPreference
- NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.