Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DeformDefinitionBuilder.ExpressionType |
DeformDefinitionBuilder.ExpressionType.EXP
Regular expression.
|
static DeformDefinitionBuilder.ExpressionType |
DeformDefinitionBuilder.ExpressionType.OPTION
Input is from a set of fixed values.
|
static DeformDefinitionBuilder.ExpressionType |
DeformDefinitionBuilder.ExpressionType.RANGE
Input is within a range of values (integer or double)
|
Modifier and Type | Method and Description |
---|---|
static DeformDefinitionBuilder.ExpressionType |
DeformDefinitionBuilder.ExpressionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DeformDefinitionBuilder.ExpressionType |
DeformDefinitionBuilder.ExpressionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DeformDefinitionBuilder.ExpressionType[] |
DeformDefinitionBuilder.ExpressionType.values()
Returns an array that contains the values for this enum.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.