public static class DeformDefinitionBuilder.ExpressionType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_EXP
Regular expression.
|
static int |
_OPTION
Input is from a set of fixed values.
|
static int |
_RANGE
Input is within a range of values (integer or double)
|
static DeformDefinitionBuilder.ExpressionType |
EXP
Regular expression.
|
static DeformDefinitionBuilder.ExpressionType |
OPTION
Input is from a set of fixed values.
|
static DeformDefinitionBuilder.ExpressionType |
RANGE
Input is within a range of values (integer or double)
|
Modifier and Type | Method and Description |
---|---|
static DeformDefinitionBuilder.ExpressionType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DeformDefinitionBuilder.ExpressionType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DeformDefinitionBuilder.ExpressionType[] |
values()
Returns an array that contains the values for this enum.
|
public static final DeformDefinitionBuilder.ExpressionType EXP
public static final DeformDefinitionBuilder.ExpressionType RANGE
public static final DeformDefinitionBuilder.ExpressionType OPTION
public static final int _EXP
public static final int _RANGE
public static final int _OPTION
public static DeformDefinitionBuilder.ExpressionType valueOf(int value)
public static DeformDefinitionBuilder.ExpressionType valueOf(String name)
public static DeformDefinitionBuilder.ExpressionType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.