Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static DatumAxisBuilder.DirectionOrientations |
DatumAxisBuilder.DirectionOrientations.PARALLEL_TO_VECTOR
Orientation parallel to Direction
|
static DatumAxisBuilder.DirectionOrientations |
DatumAxisBuilder.DirectionOrientations.PERPENDICULAR_TO_VECTOR
Orientation perpendicular to Direction
|
Modifier and Type | Method and Description |
---|---|
DatumAxisBuilder.DirectionOrientations |
DatumAxisBuilder.directionOrientation()
Returns the direction orientation.
|
static DatumAxisBuilder.DirectionOrientations |
DatumAxisBuilder.DirectionOrientations.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DatumAxisBuilder.DirectionOrientations |
DatumAxisBuilder.DirectionOrientations.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DatumAxisBuilder.DirectionOrientations[] |
DatumAxisBuilder.DirectionOrientations.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DatumAxisBuilder.setDirectionOrientation(DatumAxisBuilder.DirectionOrientations directionOrientation)
License requirements: solid_modeling ("SOLIDS MODELING") OR geometric_tol ("GDT") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.