public static class DatumAxisBuilder.DirectionOrientations extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_PARALLEL_TO_VECTOR
Orientation parallel to Direction
|
static int |
_PERPENDICULAR_TO_VECTOR
Orientation perpendicular to Direction
|
static DatumAxisBuilder.DirectionOrientations |
PARALLEL_TO_VECTOR
Orientation parallel to Direction
|
static DatumAxisBuilder.DirectionOrientations |
PERPENDICULAR_TO_VECTOR
Orientation perpendicular to Direction
|
Modifier and Type | Method and Description |
---|---|
static DatumAxisBuilder.DirectionOrientations |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DatumAxisBuilder.DirectionOrientations |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DatumAxisBuilder.DirectionOrientations[] |
values()
Returns an array that contains the values for this enum.
|
public static final DatumAxisBuilder.DirectionOrientations PARALLEL_TO_VECTOR
public static final DatumAxisBuilder.DirectionOrientations PERPENDICULAR_TO_VECTOR
public static final int _PARALLEL_TO_VECTOR
public static final int _PERPENDICULAR_TO_VECTOR
public static DatumAxisBuilder.DirectionOrientations valueOf(int value)
public static DatumAxisBuilder.DirectionOrientations valueOf(String name)
public static DatumAxisBuilder.DirectionOrientations[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.