Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static BridgeCurveBuilder.SelectedObject |
BridgeCurveBuilder.SelectedObject.ONE
input object 1 selected
|
static BridgeCurveBuilder.SelectedObject |
BridgeCurveBuilder.SelectedObject.TWO
input object 2 selected
|
Modifier and Type | Method and Description |
---|---|
BridgeCurveBuilder.SelectedObject |
BridgeCurveBuilder.objectSelectionOption()
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
static BridgeCurveBuilder.SelectedObject |
BridgeCurveBuilder.SelectedObject.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeCurveBuilder.SelectedObject |
BridgeCurveBuilder.SelectedObject.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeCurveBuilder.SelectedObject[] |
BridgeCurveBuilder.SelectedObject.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BridgeCurveBuilder.setObjectSelectionOption(BridgeCurveBuilder.SelectedObject objectSelectionOption)
Deprecated.
Deprecated in NX8.5.0. Use
BridgeCurveBuilderEx instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.