public static class BridgeCurveBuilder.SelectedObject extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ONE
input object 1 selected
|
static int |
_TWO
input object 2 selected
|
static BridgeCurveBuilder.SelectedObject |
ONE
input object 1 selected
|
static BridgeCurveBuilder.SelectedObject |
TWO
input object 2 selected
|
Modifier and Type | Method and Description |
---|---|
static BridgeCurveBuilder.SelectedObject |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeCurveBuilder.SelectedObject |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeCurveBuilder.SelectedObject[] |
values()
Returns an array that contains the values for this enum.
|
public static final BridgeCurveBuilder.SelectedObject ONE
public static final BridgeCurveBuilder.SelectedObject TWO
public static final int _ONE
public static final int _TWO
public static BridgeCurveBuilder.SelectedObject valueOf(int value)
public static BridgeCurveBuilder.SelectedObject valueOf(String name)
public static BridgeCurveBuilder.SelectedObject[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.