Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static AestheticFaceBlendBuilder.CenterType |
AestheticFaceBlendBuilder.CenterType.CENTER_RADIUS
Center radius option.
|
static AestheticFaceBlendBuilder.CenterType |
AestheticFaceBlendBuilder.CenterType.RHO
Rho is the ratio of the center radius and the base radius.
|
Modifier and Type | Method and Description |
---|---|
AestheticFaceBlendBuilder.CenterType |
AestheticFaceBlendBuilder.centerOption()
Returns the center option
License requirements: None. |
static AestheticFaceBlendBuilder.CenterType |
AestheticFaceBlendBuilder.CenterType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AestheticFaceBlendBuilder.CenterType |
AestheticFaceBlendBuilder.CenterType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AestheticFaceBlendBuilder.CenterType[] |
AestheticFaceBlendBuilder.CenterType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AestheticFaceBlendBuilder.setCenterOption(AestheticFaceBlendBuilder.CenterType centerOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.