public static class AestheticFaceBlendBuilder.CenterType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CENTER_RADIUS
Center radius option.
|
static int |
_RHO
Rho is the ratio of the center radius and the base radius.
|
static AestheticFaceBlendBuilder.CenterType |
CENTER_RADIUS
Center radius option.
|
static AestheticFaceBlendBuilder.CenterType |
RHO
Rho is the ratio of the center radius and the base radius.
|
Modifier and Type | Method and Description |
---|---|
static AestheticFaceBlendBuilder.CenterType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AestheticFaceBlendBuilder.CenterType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AestheticFaceBlendBuilder.CenterType[] |
values()
Returns an array that contains the values for this enum.
|
public static final AestheticFaceBlendBuilder.CenterType CENTER_RADIUS
public static final AestheticFaceBlendBuilder.CenterType RHO
public static final int _CENTER_RADIUS
public static final int _RHO
public static AestheticFaceBlendBuilder.CenterType valueOf(int value)
public static AestheticFaceBlendBuilder.CenterType valueOf(String name)
public static AestheticFaceBlendBuilder.CenterType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.