Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for Display.
|
Modifier and Type | Field and Description |
---|---|
static LightBuilder.ShadowType |
LightBuilder.ShadowType.HARD_EDGED
Hard-edged, precise shadows will be generated using a ray-tracing
algorithm.
|
static LightBuilder.ShadowType |
LightBuilder.ShadowType.NONE
No shadows will be produced.
|
static LightBuilder.ShadowType |
LightBuilder.ShadowType.SOFT_EDGED
Soft-edged,approximated shadows will be generated using a shadow
mapping algorithm.
|
static LightBuilder.ShadowType |
LightBuilder.ShadowType.TRANSLUCENT_HARD
Hard-edged, precise shadows will be generated using a ray-tracing
algorithm.
|
Modifier and Type | Method and Description |
---|---|
LightBuilder.ShadowType |
LightBuilder.lightShadowType()
Returns the light shadow type - not applicable to ambient or eye light types
License requirements: None. |
static LightBuilder.ShadowType |
LightBuilder.ShadowType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LightBuilder.ShadowType |
LightBuilder.ShadowType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LightBuilder.ShadowType[] |
LightBuilder.ShadowType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LightBuilder.setLightShadowType(LightBuilder.ShadowType lightShadowType)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.