Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for Display.
|
Modifier and Type | Field and Description |
---|---|
static DecalBuilder.ImageSize |
DecalBuilder.ImageSize.FIVE_TWELVE
resize image to 512 x 512
|
static DecalBuilder.ImageSize |
DecalBuilder.ImageSize.FOUR_ONINE_SIX
resize image to 4096x 4096
|
static DecalBuilder.ImageSize |
DecalBuilder.ImageSize.ONE_OTWO_FOUR
resize image to 1024 x1024
|
static DecalBuilder.ImageSize |
DecalBuilder.ImageSize.ONE_TWENTY_EIGHT
resize image to 128 x 128
|
static DecalBuilder.ImageSize |
DecalBuilder.ImageSize.TRUE_SIZE
use true image size
|
static DecalBuilder.ImageSize |
DecalBuilder.ImageSize.TWO_FIFTY_SIX
resize iamge to 256 x 256
|
static DecalBuilder.ImageSize |
DecalBuilder.ImageSize.TWO_OFOUR_EIGHT
resize image to 2048x2048
|
Modifier and Type | Method and Description |
---|---|
DecalBuilder.ImageSize |
DecalBuilder.imageSizeType()
Returns the image size type
License requirements: None. |
static DecalBuilder.ImageSize |
DecalBuilder.ImageSize.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DecalBuilder.ImageSize |
DecalBuilder.ImageSize.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DecalBuilder.ImageSize[] |
DecalBuilder.ImageSize.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DecalBuilder.setImageSizeType(DecalBuilder.ImageSize imageSizeType)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.