public static class DecalBuilder.ImageSize extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FIVE_TWELVE
resize image to 512 x 512
|
static int |
_FOUR_ONINE_SIX
resize image to 4096x 4096
|
static int |
_ONE_OTWO_FOUR
resize image to 1024 x1024
|
static int |
_ONE_TWENTY_EIGHT
resize image to 128 x 128
|
static int |
_TRUE_SIZE
use true image size
|
static int |
_TWO_FIFTY_SIX
resize iamge to 256 x 256
|
static int |
_TWO_OFOUR_EIGHT
resize image to 2048x2048
|
static DecalBuilder.ImageSize |
FIVE_TWELVE
resize image to 512 x 512
|
static DecalBuilder.ImageSize |
FOUR_ONINE_SIX
resize image to 4096x 4096
|
static DecalBuilder.ImageSize |
ONE_OTWO_FOUR
resize image to 1024 x1024
|
static DecalBuilder.ImageSize |
ONE_TWENTY_EIGHT
resize image to 128 x 128
|
static DecalBuilder.ImageSize |
TRUE_SIZE
use true image size
|
static DecalBuilder.ImageSize |
TWO_FIFTY_SIX
resize iamge to 256 x 256
|
static DecalBuilder.ImageSize |
TWO_OFOUR_EIGHT
resize image to 2048x2048
|
Modifier and Type | Method and Description |
---|---|
static DecalBuilder.ImageSize |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DecalBuilder.ImageSize |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DecalBuilder.ImageSize[] |
values()
Returns an array that contains the values for this enum.
|
public static final DecalBuilder.ImageSize TRUE_SIZE
public static final DecalBuilder.ImageSize ONE_TWENTY_EIGHT
public static final DecalBuilder.ImageSize TWO_FIFTY_SIX
public static final DecalBuilder.ImageSize FIVE_TWELVE
public static final DecalBuilder.ImageSize ONE_OTWO_FOUR
public static final DecalBuilder.ImageSize TWO_OFOUR_EIGHT
public static final DecalBuilder.ImageSize FOUR_ONINE_SIX
public static final int _TRUE_SIZE
public static final int _ONE_TWENTY_EIGHT
public static final int _TWO_FIFTY_SIX
public static final int _FIVE_TWELVE
public static final int _ONE_OTWO_FOUR
public static final int _TWO_OFOUR_EIGHT
public static final int _FOUR_ONINE_SIX
public static DecalBuilder.ImageSize valueOf(int value)
public static DecalBuilder.ImageSize valueOf(String name)
public static DecalBuilder.ImageSize[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.