Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
SelectISurface |
SketchInPlaceBuilder.planeOrFace()
Deprecated.
Deprecated in NX11.0.0. Use
SketchInPlaceBuilder.planeReference() instead.
|
Modifier and Type | Method and Description |
---|---|
SelectISurface |
DeleteFaceBuilder.capFace()
Returns the face or plane to be used as cap face.
|
SelectISurface |
MirrorFaceBuilder.existingMirrorPlane()
Returns the existing mirror plane
License requirements: None. |
SelectISurface |
MirrorCurveBuilder.existingPlane()
Returns the Mirror plane/face
License requirements: None. |
SelectISurface |
SymmetricBuilder.existingSymmetryPlane()
Returns the existing symmetry plane.
|
SelectISurface |
WrapBuilder.plane()
Returns the planar face or datum plane that the curves are being wrapped from or unwrapped to.
|
SelectISurface |
MirrorFeatureBuilder.plane()
Returns the Mirror Plane
License requirements: None. |
SelectISurface |
EditCrossSectionBuilder.plane()
Returns the select plane.
|
SelectISurface |
TangentBuilder.stationaryFace()
Returns the stationary face
License requirements: None. |
SelectISurface |
PerpendicularBuilder.stationaryFace()
Returns the stationary face
License requirements: None. |
SelectISurface |
ParallelBuilder.stationaryFace()
Returns the stationary face.
|
SelectISurface |
CoplanarBuilder.stationaryFace()
Returns the stationary face
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectISurface |
BridgeTransitionBuilder.plane()
Returns the tangential plane
Only use this option to edit feature created prior to NX12. |
Modifier and Type | Method and Description |
---|---|
SelectISurface |
MirrorPattern.existingPlane()
Returns the Existing Mirror Plane
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.