Package | Description |
---|---|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.features.sheetmetal |
Provides classes and interfaces for Sheet Metal Features.
|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
Modifier and Type | Method and Description |
---|---|
SelectEdge |
GeodesicDimensionBuilder.originCurve()
Returns the curves or edges to dimension from
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectEdge |
StyledBlendBuilder.adjacentBlend1()
Returns the first adjacent blend
License requirements: studio_free_form ("STUDIO FREE FORM") . |
SelectEdge |
StyledBlendBuilder.adjacentBlend2()
Returns the second adjacent blend
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Modifier and Type | Method and Description |
---|---|
SelectEdge |
BridgeTransitionBuilder.endEdge()
Returns the end edge
License requirements: nx_flexible_pcb ("NX Flexible PCB") OR nx_sheet_metal ("NX Sheet Metal") . |
SelectEdge |
ResizeBendAngleBuilder.referenceEdge()
Returns the reference edge
License requirements: nx_sheet_metal ("NX Sheet Metal") OR nx_flexible_pcb ("NX Flexible PCB") . |
SelectEdge |
GussetBuilder.startEdge()
Returns the start edge
Only use this option to edit gussets created prior to NX10. |
SelectEdge |
BridgeTransitionBuilder.startEdge()
Returns the start edge
License requirements: nx_flexible_pcb ("NX Flexible PCB") OR nx_sheet_metal ("NX Sheet Metal") . |
SelectEdge |
FlatSolidBuilder.xaxisEdge()
Returns the x axis edge selection
License requirements: None. |
SelectEdge |
FlatPatternBuilder.xaxisEdge()
Returns the x axis edge selection.
|
Modifier and Type | Method and Description |
---|---|
SelectEdge |
EndCutBuilder.placementEdge()
Returns the select placement edges.
|
SelectEdge |
PinJigBuilder.xdirectionEdge()
Returns the edge from the plates whose tangent should be used to define the x direction.
|
Modifier and Type | Method and Description |
---|---|
SelectEdge |
MatchSurfaceBuilder.editEdge()
Returns the selected edge for matching
License requirements: None. |
SelectEdge |
MatchSurfaceBuilder.reference()
Returns the selected reference edge or curve
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
SelectEdge |
InsertAuxiliaryBuilder.insertEdge()
Returns the insert edge.
|
SelectEdge |
InsertAuxiliaryBuilder.mountPunchEdge()
Returns the punch edge to place the mount.
|
SelectEdge |
ScrapDesignBuilder.overcutEdge()
Returns the edge that overcut will be attached
License requirements: None. |
SelectEdge |
InsertAuxiliaryBuilder.punchEdge()
Returns the punch edge.
|
SelectEdge |
SlugRetentionBuilder.slugRetentionEdge()
Returns the slug retention edge
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.