Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.features |
Provides classes and interfaces for features.
|
Modifier and Type | Field and Description |
---|---|
static HumanData.InverseKinematicsInitJoint |
HumanData.InverseKinematicsInitJoint.SHOULDER
Indicate starting at the shoulder for simple arm motions
without changing the upper body position.
|
static HumanData.InverseKinematicsInitJoint |
HumanData.InverseKinematicsInitJoint.WAIST
Indicate starting arm motion at the waist and using the
entire upper body
|
Modifier and Type | Method and Description |
---|---|
static HumanData.InverseKinematicsInitJoint |
HumanData.InverseKinematicsInitJoint.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HumanData.InverseKinematicsInitJoint |
HumanData.InverseKinematicsInitJoint.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HumanData.InverseKinematicsInitJoint[] |
HumanData.InverseKinematicsInitJoint.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
HumanData.InverseKinematicsInitJoint |
HumanBuilder.initJoint()
Returns the motion initiation joint for dynamic drag of left hand or right hand
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Modifier and Type | Method and Description |
---|---|
void |
HumanBuilder.setInitJoint(HumanData.InverseKinematicsInitJoint initJoint)
License requirements: solid_modeling ("SOLIDS MODELING"), ug_human ("Human Modelling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.