public static class HumanData.InverseKinematicsInitJoint extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_SHOULDER
Indicate starting at the shoulder for simple arm motions
without changing the upper body position.
|
static int |
_WAIST
Indicate starting arm motion at the waist and using the
entire upper body
|
static HumanData.InverseKinematicsInitJoint |
SHOULDER
Indicate starting at the shoulder for simple arm motions
without changing the upper body position.
|
static HumanData.InverseKinematicsInitJoint |
WAIST
Indicate starting arm motion at the waist and using the
entire upper body
|
Modifier and Type | Method and Description |
---|---|
static HumanData.InverseKinematicsInitJoint |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HumanData.InverseKinematicsInitJoint |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HumanData.InverseKinematicsInitJoint[] |
values()
Returns an array that contains the values for this enum.
|
public static final HumanData.InverseKinematicsInitJoint SHOULDER
public static final HumanData.InverseKinematicsInitJoint WAIST
public static final int _SHOULDER
public static final int _WAIST
public static HumanData.InverseKinematicsInitJoint valueOf(int value)
public static HumanData.InverseKinematicsInitJoint valueOf(String name)
public static HumanData.InverseKinematicsInitJoint[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.