Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
nxopen.cam.fbm |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Interface and Description |
---|---|
interface |
CAMFeature
Represents a CAM Feature
To obtain an instance of this class use FeatureRecognitionBuilder Created in NX7.5.0 |
Modifier and Type | Method and Description |
---|---|
Feature |
HoleBossSet.getFeature()
Returns the in process feature
License requirements: None. |
Feature |
Operation.insertFeature(CAMFeature tagMachiningFeature)
Insert a machining feature to machine and returns an in process feature
License requirements: cam_base ("CAM BASE") . |
Modifier and Type | Method and Description |
---|---|
Feature |
FeatureSet.createFeature(NXObject[] entities)
Creates the feature using the specified tags
License requirements: cam_base ("CAM BASE") . |
Feature[] |
FeatureGeometry.createFeatures(NXObject[] objects,
String featureType)
Create a series of (in process) features.
|
Feature |
FeatureSet.getFeature()
Returns the feature
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ThreadFeatureGeometry.updateThreadParameters(Feature tagFeature)
Update the feature thread parameters
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.