Interface | Description |
---|---|
Feature |
Interface for CAM Feature objects
This is an abstract class, and cannot be instantiated. |
FeatureGeometry |
Represents a feature geometry builder
This is an abstract class and cannot be instantiated. |
FeatureSet |
Interface for feature set
To create a new instance of this class, use FeatureGeometry.createFeatureSet() Created in NX9.0.0 |
MachiningFeatureGeometry |
Represents a feature geometry builder
An instance of this class can be obtained from HoleBossGeom.getCenterHoleGeometry() or HoleBossGeom.getChamferHoleGeometry() Created in NX9.0.0 |
ThreadFeatureGeometry |
Represents a feature geometry builder
This is an abstract class and cannot be instantiated. |
Class | Description |
---|---|
FeatureGeometry.SequenceDirectionType |
the direction types .
|
FeatureGeometry.SequencePatternType |
the pattern types .
|
FeatureGeometry.SortOrder |
the optimization types .
|
ThreadFeatureGeometry.Form |
Thread form standards .
|
ThreadFeatureGeometry.Rotation |
the rotation types .
|
ThreadFeatureGeometry.ThreadDataSource |
thread data source types .
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.