Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TurnRoughFinishLocalReturnBuilder.LimitTypes |
TurnRoughFinishLocalReturnBuilder.LimitTypes.DISTANCE_OR_TIME
mm,inch or sec
|
static TurnRoughFinishLocalReturnBuilder.LimitTypes |
TurnRoughFinishLocalReturnBuilder.LimitTypes.PERCENT
%
|
Modifier and Type | Method and Description |
---|---|
TurnRoughFinishLocalReturnBuilder.LimitTypes |
TurnRoughFinishLocalReturnBuilder.getLowerLimitType()
Get the lower limits mode
License requirements: None. |
TurnRoughFinishLocalReturnBuilder.LimitTypes |
TurnRoughFinishLocalReturnBuilder.getUpperLimitType()
Get the upper limits mode
License requirements: None. |
static TurnRoughFinishLocalReturnBuilder.LimitTypes |
TurnRoughFinishLocalReturnBuilder.LimitTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnRoughFinishLocalReturnBuilder.LimitTypes |
TurnRoughFinishLocalReturnBuilder.LimitTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnRoughFinishLocalReturnBuilder.LimitTypes[] |
TurnRoughFinishLocalReturnBuilder.LimitTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TurnRoughFinishLocalReturnBuilder.setLowerLimitType(TurnRoughFinishLocalReturnBuilder.LimitTypes lowerLimitModeValue)
Set the lower limits mode
License requirements: cam_base ("CAM BASE") . |
void |
TurnRoughFinishLocalReturnBuilder.setUpperLimitType(TurnRoughFinishLocalReturnBuilder.LimitTypes upperLimitModeValue)
Set the upper limits mode
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.