public static class TurnRoughFinishLocalReturnBuilder.LimitTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DISTANCE_OR_TIME
mm,inch or sec
|
static int |
_PERCENT
%
|
static TurnRoughFinishLocalReturnBuilder.LimitTypes |
DISTANCE_OR_TIME
mm,inch or sec
|
static TurnRoughFinishLocalReturnBuilder.LimitTypes |
PERCENT
%
|
Modifier and Type | Method and Description |
---|---|
static TurnRoughFinishLocalReturnBuilder.LimitTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TurnRoughFinishLocalReturnBuilder.LimitTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TurnRoughFinishLocalReturnBuilder.LimitTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final TurnRoughFinishLocalReturnBuilder.LimitTypes DISTANCE_OR_TIME
public static final TurnRoughFinishLocalReturnBuilder.LimitTypes PERCENT
public static final int _DISTANCE_OR_TIME
public static final int _PERCENT
public static TurnRoughFinishLocalReturnBuilder.LimitTypes valueOf(int value)
public static TurnRoughFinishLocalReturnBuilder.LimitTypes valueOf(String name)
public static TurnRoughFinishLocalReturnBuilder.LimitTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.