Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static TabPointDataBuilder.TabThreadMethodType |
TabPointDataBuilder.TabThreadMethodType.SAME_AS_TAB_START_POINT
Same as Tab start point
|
static TabPointDataBuilder.TabThreadMethodType |
TabPointDataBuilder.TabThreadMethodType.THREAD_AT_LEAD_IN
Thread at Lead-in
|
static TabPointDataBuilder.TabThreadMethodType |
TabPointDataBuilder.TabThreadMethodType.USER_DEFINED
User Defined
|
Modifier and Type | Method and Description |
---|---|
TabPointDataBuilder.TabThreadMethodType |
TabPointDataBuilder.tabThreadMethod()
Returns the tab thread method option
License requirements: cam_base ("CAM BASE") . |
static TabPointDataBuilder.TabThreadMethodType |
TabPointDataBuilder.TabThreadMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TabPointDataBuilder.TabThreadMethodType |
TabPointDataBuilder.TabThreadMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TabPointDataBuilder.TabThreadMethodType[] |
TabPointDataBuilder.TabThreadMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TabPointDataBuilder.setTabThreadMethod(TabPointDataBuilder.TabThreadMethodType threadMethod)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.