public static class TabPointDataBuilder.TabThreadMethodType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_SAME_AS_TAB_START_POINT
Same as Tab start point
|
static int |
_THREAD_AT_LEAD_IN
Thread at Lead-in
|
static int |
_USER_DEFINED
User Defined
|
static TabPointDataBuilder.TabThreadMethodType |
SAME_AS_TAB_START_POINT
Same as Tab start point
|
static TabPointDataBuilder.TabThreadMethodType |
THREAD_AT_LEAD_IN
Thread at Lead-in
|
static TabPointDataBuilder.TabThreadMethodType |
USER_DEFINED
User Defined
|
Modifier and Type | Method and Description |
---|---|
static TabPointDataBuilder.TabThreadMethodType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TabPointDataBuilder.TabThreadMethodType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TabPointDataBuilder.TabThreadMethodType[] |
values()
Returns an array that contains the values for this enum.
|
public static final TabPointDataBuilder.TabThreadMethodType SAME_AS_TAB_START_POINT
public static final TabPointDataBuilder.TabThreadMethodType USER_DEFINED
public static final TabPointDataBuilder.TabThreadMethodType THREAD_AT_LEAD_IN
public static final int _SAME_AS_TAB_START_POINT
public static final int _USER_DEFINED
public static final int _THREAD_AT_LEAD_IN
public static TabPointDataBuilder.TabThreadMethodType valueOf(int value)
public static TabPointDataBuilder.TabThreadMethodType valueOf(String name)
public static TabPointDataBuilder.TabThreadMethodType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.