Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static SimulationOptionsBuilder.Enable |
SimulationOptionsBuilder.Enable.NO
no
|
static SimulationOptionsBuilder.Enable |
SimulationOptionsBuilder.Enable.YES
yes
|
Modifier and Type | Method and Description |
---|---|
SimulationOptionsBuilder.Enable |
SimulationOptionsBuilder.enableCollision()
Returns the enable collision
License requirements: None. |
SimulationOptionsBuilder.Enable |
SimulationOptionsBuilder.enableDisplay()
Deprecated.
Deprecated in NX10.0.2. Use
SimulationOptionsBuilder.simulationDisplay() instead.
|
static SimulationOptionsBuilder.Enable |
SimulationOptionsBuilder.Enable.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimulationOptionsBuilder.Enable |
SimulationOptionsBuilder.Enable.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimulationOptionsBuilder.Enable[] |
SimulationOptionsBuilder.Enable.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SimulationOptionsBuilder.setEnableCollision(SimulationOptionsBuilder.Enable enableValue)
License requirements: ug_isv_full ("Full functionality for Integrated Simulation and Verification") . |
void |
SimulationOptionsBuilder.setEnableDisplay(SimulationOptionsBuilder.Enable enableValue)
Deprecated.
Deprecated in NX10.0.2. Use
SimulationOptionsBuilder.setSimulationDisplay(nxopen.cam.SimulationOptionsBuilder.SimulationDisplayMode) instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.