public static class SimulationOptionsBuilder.Enable extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NO
no
|
static int |
_YES
yes
|
static SimulationOptionsBuilder.Enable |
NO
no
|
static SimulationOptionsBuilder.Enable |
YES
yes
|
Modifier and Type | Method and Description |
---|---|
static SimulationOptionsBuilder.Enable |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimulationOptionsBuilder.Enable |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimulationOptionsBuilder.Enable[] |
values()
Returns an array that contains the values for this enum.
|
public static final SimulationOptionsBuilder.Enable NO
public static final SimulationOptionsBuilder.Enable YES
public static final int _NO
public static final int _YES
public static SimulationOptionsBuilder.Enable valueOf(int value)
public static SimulationOptionsBuilder.Enable valueOf(String name)
public static SimulationOptionsBuilder.Enable[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.