Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static RoughFinishTurningBuilder.MinmaxSizeModes |
RoughFinishTurningBuilder.MinmaxSizeModes.AXIAL
Axial
|
static RoughFinishTurningBuilder.MinmaxSizeModes |
RoughFinishTurningBuilder.MinmaxSizeModes.AXIAL_AND_RADIAL
Axial and Radial
|
static RoughFinishTurningBuilder.MinmaxSizeModes |
RoughFinishTurningBuilder.MinmaxSizeModes.NONE
None.
|
static RoughFinishTurningBuilder.MinmaxSizeModes |
RoughFinishTurningBuilder.MinmaxSizeModes.RADIAL
Radial
|
Modifier and Type | Method and Description |
---|---|
RoughFinishTurningBuilder.MinmaxSizeModes |
RoughFinishTurningBuilder.maximumSizeMode()
Returns the Maximum Size Mode
License requirements: None. |
RoughFinishTurningBuilder.MinmaxSizeModes |
RoughFinishTurningBuilder.minimumSizeMode()
Returns the Minimum Size Mode
License requirements: None. |
static RoughFinishTurningBuilder.MinmaxSizeModes |
RoughFinishTurningBuilder.MinmaxSizeModes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RoughFinishTurningBuilder.MinmaxSizeModes |
RoughFinishTurningBuilder.MinmaxSizeModes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RoughFinishTurningBuilder.MinmaxSizeModes[] |
RoughFinishTurningBuilder.MinmaxSizeModes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RoughFinishTurningBuilder.setMaximumSizeMode(RoughFinishTurningBuilder.MinmaxSizeModes maximumSizeMode)
License requirements: cam_base ("CAM BASE") . |
void |
RoughFinishTurningBuilder.setMinimumSizeMode(RoughFinishTurningBuilder.MinmaxSizeModes minimumSizeMode)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.