Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static RoughFinishTurningBuilder.MinmaxAreaUnits |
RoughFinishTurningBuilder.MinmaxAreaUnits.PERCENTAGE
Percentage
|
static RoughFinishTurningBuilder.MinmaxAreaUnits |
RoughFinishTurningBuilder.MinmaxAreaUnits.SQUARE
Square length.
|
Modifier and Type | Method and Description |
---|---|
RoughFinishTurningBuilder.MinmaxAreaUnits |
RoughFinishTurningBuilder.maximumAreaUnit()
Returns the Maximum Area Unit
License requirements: None. |
RoughFinishTurningBuilder.MinmaxAreaUnits |
RoughFinishTurningBuilder.minimumAreaUnit()
Returns the Minimum Area Unit
License requirements: None. |
static RoughFinishTurningBuilder.MinmaxAreaUnits |
RoughFinishTurningBuilder.MinmaxAreaUnits.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static RoughFinishTurningBuilder.MinmaxAreaUnits |
RoughFinishTurningBuilder.MinmaxAreaUnits.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static RoughFinishTurningBuilder.MinmaxAreaUnits[] |
RoughFinishTurningBuilder.MinmaxAreaUnits.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
RoughFinishTurningBuilder.setMaximumAreaUnit(RoughFinishTurningBuilder.MinmaxAreaUnits maxAreaUnit)
License requirements: cam_base ("CAM BASE") . |
void |
RoughFinishTurningBuilder.setMinimumAreaUnit(RoughFinishTurningBuilder.MinmaxAreaUnits minAreaUnit)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.