Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static NcmWedmBuilder.NonTiltLeadInTypes |
NcmWedmBuilder.NonTiltLeadInTypes.FOUR_AXIS
non-tilt lead in type 4-axis
|
static NcmWedmBuilder.NonTiltLeadInTypes |
NcmWedmBuilder.NonTiltLeadInTypes.ZM
non-tilt lead in type zm
|
Modifier and Type | Method and Description |
---|---|
NcmWedmBuilder.NonTiltLeadInTypes |
NcmWedmBuilder.nonTiltLeadIn()
Returns the non_tilt_lead_in
License requirements: cam_base ("CAM BASE") . |
static NcmWedmBuilder.NonTiltLeadInTypes |
NcmWedmBuilder.NonTiltLeadInTypes.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NcmWedmBuilder.NonTiltLeadInTypes |
NcmWedmBuilder.NonTiltLeadInTypes.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NcmWedmBuilder.NonTiltLeadInTypes[] |
NcmWedmBuilder.NonTiltLeadInTypes.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NcmWedmBuilder.setNonTiltLeadIn(NcmWedmBuilder.NonTiltLeadInTypes nonTiltLeadIn)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.