public static class NcmWedmBuilder.NonTiltLeadInTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FOUR_AXIS
non-tilt lead in type 4-axis
|
static int |
_ZM
non-tilt lead in type zm
|
static NcmWedmBuilder.NonTiltLeadInTypes |
FOUR_AXIS
non-tilt lead in type 4-axis
|
static NcmWedmBuilder.NonTiltLeadInTypes |
ZM
non-tilt lead in type zm
|
Modifier and Type | Method and Description |
---|---|
static NcmWedmBuilder.NonTiltLeadInTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NcmWedmBuilder.NonTiltLeadInTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NcmWedmBuilder.NonTiltLeadInTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final NcmWedmBuilder.NonTiltLeadInTypes ZM
public static final NcmWedmBuilder.NonTiltLeadInTypes FOUR_AXIS
public static final int _ZM
public static final int _FOUR_AXIS
public static NcmWedmBuilder.NonTiltLeadInTypes valueOf(int value)
public static NcmWedmBuilder.NonTiltLeadInTypes valueOf(String name)
public static NcmWedmBuilder.NonTiltLeadInTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.