Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Interface and Description |
---|---|
interface |
CavityMilling
Represents a Cavity Milling Operation
To create or edit an instance of this class, use CavityMillingBuilder Created in NX7.5.0 |
interface |
Engraving
Represents a Engraving Operation
To create or edit an instance of this class, use EngravingBuilder Created in NX7.5.0 |
interface |
FaceMilling
Represents a Face Milling Operation
To create or edit an instance of this class, use FaceMillingBuilder Created in NX7.5.0 |
interface |
FeatureMilling
Represents a Feature Milling Operation
To create or edit an instance of this class, use FeatureMillingBuilder Created in NX7.5.0 |
interface |
GrooveMilling
Represents a Groove Milling Operation
To create or edit an instance of this class, use GrooveMillingBuilder Created in NX9.0.0 |
interface |
PlanarMilling
Represents a Planar Milling Operation
To create or edit an instance of this class, use PlanarMillingBuilder Created in NX7.5.0 |
interface |
PlanarOperation
Represents a Planar operation
To create or edit an instance of this class, use PlanarOperationBuilder Created in NX7.5.0 |
interface |
PlungeMilling
Represents a Plunge Milling Operation
To create or edit an instance of this class, use PlungeMillingBuilder Created in NX7.5.0 |
interface |
SurfaceContour
Represents a Surface Contour operation
To create or edit an instance of this class, use SurfaceContourBuilder Created in NX7.5.0 |
interface |
VariableZLevelMilling
Represents a Variable Z Level Milling Operation
To create or edit an instance of this class, use VazlMillingBuilder Created in NX7.5.0 |
interface |
VolumeBased25DMillingOperation
Represents a Floor Wall Milling Operation
To create or edit an instance of this class, use VolumeBased25DMillingOperationBuilder Created in NX8.5.0 |
interface |
ZLevelMilling
Represents a Z Level Milling Operation
To create or edit an instance of this class, use ZLevelMillingBuilder Created in NX7.5.0 |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.